This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24104充电过程中stat1的灯在闪烁



我用BQ240104充3.7V,6600mAH的锂电池组,充电电流设计1.6A(实际1.5A),充电截止电流设置0.445A(实际0.387A)。

在实际充电过程中当电池充电充了4小时24分钟后,stat1所连接的发光lED灯就开始闪烁了。不管我拔电池、拔DC输入或者重新上电,都无法让这个状态恢复。下图是我的原理图。

最开始我根据这个芯片的数据手册来排查,

在出现闪烁时, 电池的电压我,测量,是4.04V,所以应该不是Battery over discharge的问题。充电闪烁时候,电池和板子的温度都比较低,所以应该不是触发了过温保护,由于充电阶段是在fast charge阶段,所以,应该是不precharge time fault。所以我就怀疑是 Fast charge timer fault,我之前是用0.1uf的,根据数据手册计算,应该是4.3小时,但是我用两个0.1uf的电容并起来,理论应该有近9个小时,但是发现,充电4个半小时左右,还是出现了这个问题。目前总共遇到了3次左右,都是大概在这个时间点出现问题。