Other Parts Discussed in Thread: LMV431,
在测试LM25117手册推荐的利用LMV431实现恒流的方案,恒流也比较稳定,但碰到一个问题:DC输入是24V,输出电压最高被限制在13V,上不去了,负载为30Ω电阻;把负载调整为50Ω电阻时,输出电压变为15V。检查上管驱动脉宽46.65%且很稳定,基本确定脉宽被限制了,类似于逐周波限制,但测试FB引脚电压(电压反馈)只有0.4V,Cramp三角波最高0.6V,也没有到1.2V限值,LMV431参考端电压0.5V左右,8550也没有打开,Rs为5mΩ,改为2.5mΩ也没变化。当前频率为100kHz。麻烦给分析分析是什么原因导致的?