This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS40210电路不稳定状况请教

Other Parts Discussed in Thread: TPS61175, TPS40210

之前用TPS61175做的板子,电压纹波大,而且不稳定

改用TPS40210之后,图见附件,存在以下问题,请高手指教:

输入电压7.4V锂电,输出电压18.2V/2A,目的是为了驱动串接的6颗LED灯。

问题

1、空载状况,输出电压正常

2、增加负载,电压基本稳定(示波器测试),偶尔有0.5V波动,回路电流持续增加,初始电流越大,电流增加越多

3、回路电流调节至1.2A以上,大概持续30s~60s,输出电压就会降低至14.5V左右,LED灯灭,断电后上电,输出电压正常

4、偶尔,在负载状况下,输出电压不变,电流突然增大至3A以上……

是电路元件没配好么?