This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
选择因素是什么
与VCC
很普通的肖特基就行了,主要关注耐压,最高反压应该是上管开通时的VIN+CBOOT吧,再留些余量。二极管作用是下管导通时给CBOOT充电,CBOOT电容是驱动上管用的,所以功率很小。
表上说Cboot最大15V,这个电压怎么知道大概多少呢
当我输入24V 输入电流可调时,输出12.6V 电流3A时 按照计算参数所得的电路一切正常,但是当我输出12.6V电流6A时,电路会出现输入电流满载输出,输出电压由24V低至14V,请问为什么啊