在使用电源管理IC TPS65311时,发现系统上电后如果没有给WD引脚喂狗的话,Watch dog 会发出复位信号。可这时我的CPU都没有程序,因此也是无法喂狗的,导致CPU下载程序都成问题。请问有什么办法可以解决这个问题吗,比如把Watch dog 关闭,但从数据手册上看 没有说关闭watch dog 的方法。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用电源管理IC TPS65311时,发现系统上电后如果没有给WD引脚喂狗的话,Watch dog 会发出复位信号。可这时我的CPU都没有程序,因此也是无法喂狗的,导致CPU下载程序都成问题。请问有什么办法可以解决这个问题吗,比如把Watch dog 关闭,但从数据手册上看 没有说关闭watch dog 的方法。
RESN and PRESN must keep the main processor and peripheral devices in a defined state during power up and power down in case of improper supply voltages or a critical failure condition. Therefore, for low supply voltages the topology of the reset outputs specify that RESN and PRESN are always held at a low level when RESN and PRESN are asserted, even if VIN falls below VPOR or the device is in SHUTDOWN mode.
datasheet里描述在电源上电期间,RESN 与PRESN会一直被拉低,这个时候watchdog复位信号的优先级应该没这个高。