This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25619E: BQ25619E REGN PIN output voltage out of spec & whether it can be replaced by peripherals power supply? BQ25619E REGN脚电压超规,是否可以使用外部电源替代来检测NTC?

Part Number: BQ25619E
Other Parts Discussed in Thread: BQ25619,

We used the BQ25619E chip in our product for Li-on battery charging power management with the BQ25619 internal NTC temperature controlling, NTC pull up to REGN power.
We also measurement the NTC by MCU ADC port for software parallel protection.
But after measurement, we found the REGN voltage not same as specification claim. When USB Vbus is 5.5V as USB2.0 protocol up limitation, the REGN is 5.4V. When USB Vbus is 5.0V, the REGN is 4.9V rather than 4.8V. the REGN has too much fluctuation and caused software parallel big error.
So we wondering know, whether we can use a fixable 3.3V power rather than REGN power, for BQ25619E chip NTC detection.
Thanks for answer.
我们在产品中使用了BQ25619E芯片用于锂电池充电电源管理并且也使用了BQ25619内置的NTC温度控制,NTC端按照规格书推荐拉高到REGN电源。
我们还通过MCU ADC端口测量NTC,以实现软件并行保护。
但经过测量,我们发现REGN电压与规格宣传不符。当USB Vbus为5.5V作为USB2.0协议上限时,REGN为5.4V。当USB Vbus为5.0V时,REGN为4.9V而不是4.8V。REGN波动过大,导致软件并行误差较大。
所以我们想知道,我们是否可以使用可固定的3.3V电源,而不是REGN脚电压,来进行BQ25619E芯片NTC检测。
谢谢你的回答。