This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21732QDWEVM-025: UCC21732QDWEVM-025

Part Number: UCC21732QDWEVM-025
Other Parts Discussed in Thread: UCC21750QDWEVM-025

Hi I am doing some testing with UCC21732QDWEVM-025. For the input switching, I tied IN+ to vcc and use function wave generator drive the IN- (the square wave with gnd and vcc signal level ). However whenever connect the wave generator with IN- pin, the measured IN- signal amplititude attenuated by half and the driver output (GATErefer to COM) is VEE. When I use a DC supply to drive the IN-, the current seen on the DC supply is ~70mA, whcih absolutely shows something wrong.

I have the same issue with UCC21750QDWEVM-025.