This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24171 STAT引脚闪烁

Other Parts Discussed in Thread: BQ24171

我使用BQ24171充电芯片,给三串两并的电池充电,电池标准电压是11.1V,充电最高可以达到12.6V,我发现电池快充满的时候,STAT引脚开始出现高低电平,我用直流电源15V供电,电流在0.16A到0,跳变,感觉是在充电和截止之间跳变,请问是什么原因?我看规格书跳变的原因有几个,输入过压,电池过压,时钟错误,电池不在,电池温度过高,我觉得这几个都可以排除的,我测试TS引脚是1.9V。还有一个charge suspend , 什么原因会导致这个?各位大侠帮忙分析一下,谢谢!我做了几块板子,不是所有的板卡都这样

  • 尝试把CC电流设置成一个比较小的值,看看是否有所改善。

    观察到的STAT pin高低电平的频率是否为0.5HZ?谢谢

  • STAT引脚高低电平不是0.5HZ,有时候不跳变,有时候跳变,看电流就知道一会充电一会停止,这样不断反复

  • 你好,我是按照BQ24171的第二个电路进行测试的

    我的原理图如下:

    但是,我测试的时候,插上USB5V供电,STAT引脚闪动,有时候过一会儿闪烁,但是插上单节锂电池之后就不闪烁了,而是常亮标识正在充电,但是我测量10mΩ电阻上的电压只有0.56V,也即只有56mA电流充电,我尝试增大ISET电压,没有任何变化。输入部分,AVCC的电压是5.1V,PVCC的电压是4.92V,温度测量TS部分并联了10KΩ电阻,使他在正常范围内。请问为什么充电电流这么小?怎么解决这个问题呢?