Other Parts Discussed in Thread: BQ25750
dear TIer:
我最近在设计一个工业用控制单元,电源部分需要实现如下功能:
外部12V电源输入,内部有一节锂电池做备用电源。
当外部12V掉电,BQ24193实现锂电池升压对外输出12V。
我的问题是:需要实现12V输出的接插件反插防止故障的功能。考虑到12V是双向的,所以二极管方案不太好。请问是否有合理方案实现。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ24193实现锂电池升压对外输出12V。
需要澄清的是,BQ24193可以将OTG升压至5V
需要实现12V输出的接插件反插防止故障的功能。考虑到12V是双向的,所以二极管方案不太好。请问是否有合理方案实现。
为了确认我理解正确,您是在谈论当外部12V以相反极性连接时的保护吗?您可以尝试参考此应用程序说明,了解FET驱动的反向极性保护: