Part Number: UCC2897A
设计一款36 -100VDC输入,12V, 30A输出电源,空载,较大负载工作都是正常的, 但偶然发现带60mA左右的小电流时,输出电压会跳动,进一步发现:IC处于一种: 工作 -- 停止 ---工作的反复中,再进一步发现工作若干周期后,VFB会低于2.4V导致停止PWM输出,等输出电压降到接近于0后,又会开始工作
是什么方面做错误了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
8.3.1.9 FB FB and SS/SD interact. The one with the lower-voltage value takes control on the duty cycle, refer to SS/SD description. This pin is an input for the control voltage of the pulse-width modulator of the UCC2897A.The control voltage is generated by an external-error amplifier by comparing the output voltage of the converter to a voltage reference and employing the compensation for the voltage-regulation loop. Usually, the error amplifier is located on the secondary side of the isolated-power converter and the output voltage is sent across the isolation boundary by an optocoupler. Thus, the FB pin is usually driven by the optocoupler. An external-pullup resistor to the VREF pin (pin 4) is also required for proper operation as part of the feedback circuitry. The control voltage is internally buffered and connected to the PWM comparator through a voltage divider to make it compatible to the signal level of the current-sense circuit. The useful voltage range of the FB pin is between approximately 2.5 V and 4.5 V. Control voltages below the 2.5-V threshold result in zero-duty cycle (pulse skipping) while voltages above 4.5 V result in full-duty-cycle (DMAX) operation.
这个部分有相关说明,关于您这部分,建议避免在这个范围去应用。
关于如何匹配请您参考一下工具。
https://www.ti.com.cn/tool/cn/download/SLUC662
关于验证
您好
比如只有30mA电流时怎么样避免VFB降到2.4V以下? 是因为元件配置不当而导致VFB<=2.4V?
关于如何匹配请您参考一下工具。
https://www.ti.com.cn/tool/cn/download/SLUC662
关于验证
在这种情况下,建议通过官方工具基于您实际情况做调整进行避免触发这种情况。