BQ24130 datasheet page 9电路中CMOD接地,描述中标称充电电流2A,page 14中描述,CMOD pin接地,充电电流将是iset2的precharge 0.2A,故请问此电路中2A充电电流是如何实现的。
另外,如果电路设计为1节电池充电,当电池电压小于3V时进入precharge,高于3V时进入fast charge,则CMOD是该接地还是拉高?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ24130 datasheet page 9电路中CMOD接地,描述中标称充电电流2A,page 14中描述,CMOD pin接地,充电电流将是iset2的precharge 0.2A,故请问此电路中2A充电电流是如何实现的。
另外,如果电路设计为1节电池充电,当电池电压小于3V时进入precharge,高于3V时进入fast charge,则CMOD是该接地还是拉高?
liu henry,
对于CMOD的使用,在数据手册中第2页有如下描述:
Charge mode selection: low (pull down to AGND) for pre-charge current as set by ISET2 pin and high (pull up to VREF) for fast charge current as set by ISET1 pin. If the battery voltage reaches the voltage regulation set point, IC changes to voltage regulation mode regardless of CMOD pin input.
对于充电电流的描述,请见第14页的Battery Current Regulation部分,COMD接地,如果是接10毫欧的电阻,根据公式2,预充电电流将限制在2A。并不是所说的0.2A。
CMOD接高还是接低,要看你自己的要求,是要限制快充电流还是预充电流的大小。与充电电压阀值无关。