This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24130 CMOD set

Other Parts Discussed in Thread: BQ24130

BQ24130 datasheet page 9电路中CMOD接地,描述中标称充电电流2A,page 14中描述,CMOD pin接地,充电电流将是iset2的precharge 0.2A,故请问此电路中2A充电电流是如何实现的。

另外,如果电路设计为1节电池充电,当电池电压小于3V时进入precharge,高于3V时进入fast charge,则CMOD是该接地还是拉高?

  • liu henry,

    对于CMOD的使用,在数据手册中第2页有如下描述:

    Charge mode selection: low (pull down to AGND) for pre-charge current as set by ISET2 pin and high (pull up to VREF) for fast charge current as set by ISET1 pin. If the battery voltage reaches the voltage regulation set point, IC changes to voltage regulation mode regardless of CMOD pin input.

      对于充电电流的描述,请见第14页的Battery Current Regulation部分,COMD接地,如果是接10毫欧的电阻,根据公式2,预充电电流将限制在2A。并不是所说的0.2A。

    CMOD接高还是接低,要看你自己的要求,是要限制快充电流还是预充电流的大小。与充电电压阀值无关。

  • 其他充电IC,电池电压低时进入pre-charger,充到3V再进入fast charger,经了解,24130这颗是没有此功能的了;

    另外还有个问题,STAT pin的描述中,HIGH when charger complete or SLEEP mode,规格书中没有定义在什么条件下charger complete,

    比如说充电电流小于50mA等条件,规格书中均没有定义,经实际测试,也是一直充,stat pin不会变高电平。

  • 有BQ24130的原理图库和PCB库吗?

    麻烦发一下给我

    261433241@qq.com

  • 你好!我也发现以上的问题。STAT pin脚没有充电完成的状态切换,无论充多久状态都不变!希望能得到原厂的问题反馈和帮助!