请问TI有没有芯片可以支持以下电路设计的:
输入为+4~+6V;
输出为+16~+18V(0.2mA)和-16~-18V(0.1mA)。或者只输出-16~-18V(0.1mA)。
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
或者类似的芯片,TPS61093, Datasheet 上也有参考电路。
你好 看到你是ti的员工,现在有LED电源上的问题想问你,TPS61043芯片手册上说,输出电压的范围是Vin到18V,现在我想让输出电压为5V,怎么设置,我在芯片手册上没有看到设置输出电压,输出电压可调的吗