This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25570: 设置MPPT的问题,期望是0.9,实际是0.75

Part Number: BQ25570


您好,我需要设置Vmpp=0.9Voc,使用VIN_DC分压,原理图如下。实际测的大概是0.75,达不到0.9,请问是啥原因。

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 数据表规定了10mA电流消耗下最大10%MPP调节,因此0.9V*(1-0.9)=0.81V是最坏的情况,忽略了1%的电阻容差效应。如果你考虑到1%的电阻容差,并且有1%的高R1和1%的低R2和R的最坏组合?,设定点可以低至0.73V。然而,我认为这里的情况并非如此。我怀疑C5电容器电压下降。那个盖子必须具有非常低的泄漏=高绝缘电阻=高额定电压。如果你把电容器换成50V的额定电容,监管可能会得到改善。

  • 您好,

    1,我未找到数据表对应的电流和,MPP调节的说明文字,麻烦给指出是哪个文件,在哪个章节。

    2,如果电流对应20mA,50mA,80mA,100mA,,那MPP调节是多少呢。

    3,我的太阳能光伏板有3组,每组的位置和光照不一样,导致每组光伏板的电压电流不一样,为了达到光伏板功率使用率最大化,如何设计电路呢?比如,在某一时刻,光伏板1是3V,光伏板2是2.5V,光伏板3是1.8V,是否可以实现这三路同时给MPPT供电,或者通过啥方式实现最大化选择供电?