This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ500212A 无线充电TX技术问题



您好!

我参考BQ500212AEVM-550的电路做了一个无线充电的TX板,在测试的过程中发现,无法检测到接收线圈,

无法进行充电,同时Sleep和SNOOZE都没有输出CLK信号,PWM信号有输出,更换外购的TX板就可以检测

到接收,充电也正常,不知道是什么原因造成的,麻烦您帮忙分析一下,感谢!

  • 正常上电后,500ms后,snooze引脚由低电平拉高到3.3v,之后驱动MOS管关断3.3v供电。之后snooze经过10us左右,被拉低。由此反复。

    sleep引脚一直低电平,当充电完成后会输出高电平。

    这地方有问题,查找snooze_cap、snooze_chg的外围电路。

    另外,你自己的板子是几层的?

    我也有bq500212的问题想咨询你。方便加我qq51425111.我的板子tx发射频率一直是100kHz,无法改变,也通讯不上。

  • snooze_cap. snooze_chg的外围电路简单的不能再简单了呀,我的也是这个问题,感觉类似调试MCU系统没起振工作一样!