Other Parts Discussed in Thread: BQ79616
TI的工程师好,我最近用电阻板分压来模拟电池,测试BQ79616的电压采集精度。
测试发现:
1、分压电阻用100Ω的时候可以正确采集到电阻两端的电压。(这个也是TI提供的评估版上焊的电阻值)
2、如果电阻换成1MΩ,则AFE采集不到电阻两端的电压(读到的数据是0或者很大的数据),这是为什么呢?
3、把分压电阻换成10kΩ的时候,afe可以采集到电压,但是采集的电压不对,并且采集到的值是从低串数到高串数逐渐增大(实际板子上电阻两端的分压值是3100mv,采集到的值cell1是2995mv,cell2是3054mv,cell3是3126mv,cell4是3196mv...)。为什么会出现这个现象?
下图是电阻分压模拟电池的电路,期待您的解答,谢谢!