Part Number: LMR33640
HI,TI Genius,
我在使用LMR33640设计个电路,使用IBB拓扑设计输入电压为18V,输出为-15V,输出电流为1.5A,开关频率为1MHZ;麻烦帮忙看下怎么准确评估IC的温升,官方一般是怎么评估的?是否有相关资料?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMR33640
HI,TI Genius,
我在使用LMR33640设计个电路,使用IBB拓扑设计输入电压为18V,输出为-15V,输出电流为1.5A,开关频率为1MHZ;麻烦帮忙看下怎么准确评估IC的温升,官方一般是怎么评估的?是否有相关资料?
谢谢
我已经分析了这个问题。从给出的信息来看,这是一个合适的设备。
在IBB中,电感器电流高于实际输出电流,IL=Iload(1+|VOUT|/(VIN*eff.))。你计算得对。在您的情况下,电流为3.285A,在设备的限制范围内。LMR33640的最大输出电流为4A。
谢谢和问候,