Other Parts Discussed in Thread: BQ78350, BQ76200, BQ76930
After replacing the battery cells, the PF cannot be cleared and the charging and discharging function cannot be activated.
cell 1 voltage 3964 mV
cell 2 voltage 3968 mV
cell 3 voltage 3964 mV
cell 4 voltage 3972 mV
cell 5 voltage 3960 mV
cell 6 voltage 3968 mV
cell 7 voltage 3949 mV
cell 8 voltage 3968 mV