This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问LM3481能否做电压正压转负压设计

Other Parts Discussed in Thread: LM3481, TPS5430

请问LM3481能否做电压正压转负压设计,输入24V,输出-24V,我看手册上没有,但是逻辑上是不是可以啊

  • LM3481是低侧N-MOSFET结构,由于是N_MOSFET的开关,所以这个开关类型和位置决定了如果它放在buck或inverting架构中,将无法驱动N-MSOFET,因为在buck或inverting结构中开关节点的电压在N-MOSFET打开的过程中,随着N-MSOFET对二极管电流分流,节点电压逐渐上升为Vin,所以由于没有自举驱动电路,N_MSOFET架构的LM34981不能用来做反向。它只能用做boost及其衍生的拓扑。而N-mosfet的buck DC_DC转换器可以用来做inverting,只不过需要保证输入电压与输出电压绝对值的和小于芯片Vin能够承受的最大电压,另外一种基于buck电路实现inverting的思想,是用工作于CCM模式下buck PWM信号驱动一个工作于DCM模式下的inverting ,这种模式下,输出电压能够有很好的线性调整,但不适合负载调整比较大的应用场合。

    关于您的供电要求,如果负载要求比较小,可以考虑用一个运放搭建反相器得到干净的-24v。这是最为简单可靠的负电压方案,但如果你的-24v 要求的负载以及调整率非常小,而你的24是利用LM3481这样的boost转换器升压得到的,那么我们可以在boost的开关节点上节一个耐压的小电容,比如0.1uf,这个电容通过一个肖特基二极管接到GND(二极管阳极接开关节点,阴极接GND),同时我们用一个肖特基二极管的阴极接开关节点,阳极接-24V的输出端,-24V的输出接一个电容到GND。这样就实现了一个未调整的-24V电压,它在一定的负载范围内可以维持-24v的电压。

  • 可以使用buck 芯片做Inverting Buck-boost,这个转变相当于48V转24V,所以要用高压的IC,  如LM557X LM500X 系列。

    可以参考TPS5430的使用:www.ti.com.cn/.../slvu243.pdf