This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79758-Q1: ASILD AFE's application for ASILC/ASILD 48V/12V BMS in automotive

Part Number: BQ79758-Q1

This AFE is ASILD integrity, when we do the 48V/12V BMS ASILC/ASILD function design for voltage/current/temperature sampling, Is it necessary to use redundant AFEs ? If the independent AFEs can ensure the redundant design and diagnosis of voltage/current/temperature sampling(compliance to ISO26262-5:2018 Appendix D table D.9)?