This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM65645-Q1: LM65645-Q1

Part Number: LM65645-Q1


您好,

我目前正在尋找具有最佳EMI設計的產品,並發現了LM65645-Q1。

我想詢問有關LM65645-Q1展頻功能的問題:為什麼標準低頻調變模式會以12kHz的調變頻率,將切換頻率展開±5%;而寬低頻調變模式則以6kHz的調變頻率,將切換頻率展開±10%?

(1) 關於6kHz的調變頻率,是否會受到CISPR25 RBW = 9kHz的影響,導致EMI效果不佳?

(2) 先前的DRSS技術文件提到,10kHz至16kHz之間的隨機FM可以降低音頻影響。這次選擇固定6kHz和12kHz頻率的原因是什麼?