Hello! Question 1: This specification document does not mention the gate driver driving capability and time of the TPS61289 transistor. I need to know its gate drive internal resistance and driving current in order to make a selection. Question 2: The rated current of this chip is 20A. If the current-limiting resistor is 10K, will it still trigger the 20A overcurrent protection? Question 3: Can the chip's VCC be externally powered and does supplying 6.5V to it have any impact on the internal components? Thank you