I have a BQ25730EVM and I want it to output 16.8V15A. How can I set it?
I have tested that the output can only reach 10A.
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a BQ25730EVM and I want it to output 16.8V15A. How can I set it?
I have tested that the output can only reach 10A.
Thank you!
Hi,
The board could hit input current limit. Could you try below register settings with input current limit/protection disabled?
* Created: Thu Jul 24 09:50:03 CDT 2025
*
* Format: Register Name tab Character,\t Hexadecimal register value.
* Device: bq2573x
* BQZ Container: Charger_1_00-bq2573x.bqz
*
Charge Option 0 870C
Charge Current 0000
Max Charge Voltage 20D0
OTG Voltage 09C4
OTG Current 3C00
Input Voltage 3A80
Min System Voltage 4200
IIN_HOST 7F00
Charger Status 8000
Prochot Status B800
IIN_DPM 2000
ADC VBUS and PSYS CB00
ADC IBAT 0000
ADC IIN and CMPIN 0000
ADC VSYS and VBAT 0000
Manufacture ID D540
Device ID 00D5
Charge Option 1 3F00
Charge Option 2 0005
Charge Option 3 043C
Prochot Option 0 4A81
Prochot Option 1 41A0
ADC Option 2000
Charge Option 4 0048
Vmin Active Protection 006C