原理图如下:

情况是这样的:前级BPS_15V可以带动后级负载(15V*6*0.3A=27W),但是接了该芯片后带不动后级负载(15V*6*0.05A=4.5W)。
原本认为是ILIM功能导致的,但是100K的RLIM条件下可以带的动 15V*4*0.05A=3W的负载,带 15V*5*0.05A=3.75W的负载存在负载电压下降的情况。
将RLIM从100K降低至50K后P15V的电压在0-3V跳动。
请帮帮我QAQ,很感谢能够提供帮助的各位。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
原理图如下:

情况是这样的:前级BPS_15V可以带动后级负载(15V*6*0.3A=27W),但是接了该芯片后带不动后级负载(15V*6*0.05A=4.5W)。
原本认为是ILIM功能导致的,但是100K的RLIM条件下可以带的动 15V*4*0.05A=3W的负载,带 15V*5*0.05A=3.75W的负载存在负载电压下降的情况。
将RLIM从100K降低至50K后P15V的电压在0-3V跳动。
请帮帮我QAQ,很感谢能够提供帮助的各位。
您好
你的意思是负载电流需要大于1.8A才能够正常使用吗?
不,不是负载电流,而是设定的电流限制应大于负载电流。
42K是指R296处的电阻阻值吗?我们之前试过38K的电阻,仍然达不到我们需要的电压值
是的,我指的是R296。38k本应奏效。
我刚刚意识到一件事。C316为10uF。他们能在这里使用10nF吗。使用10uF,启动将非常缓慢(需要12-13秒才能启动)