This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2057T

Other Parts Discussed in Thread: BQ24133

   请问BQ2057T芯片,是升压的还是降压的?5V输入电压,可以输出8.2V给两节锂电池充电吗?急...

  • BQ2057T是线性充电器,是降压结构,不能把5V升压到8.2V给两节锂电池充电。谢谢!

  • 如果要用5v给两节串联锂电池充电,可能的方式有

    1,升压boost dc-dc转换器将5v升压到高于8.2V电压,然后再使用BQ2057T或其他支持两节电池充电的充电器芯片,但需要注意由于使用了boost电路,所以5v输入源的电流输出能够转换为真实充电电流的部分有限,CC电流将小于5v的最大输出电流能力,同时因为考虑到升压转换和降压转换的效率,整体效率将比较低,但在5V输入源电流能力充分保障的情况下,充电时间比较短。

    2,升压boost dc-dc转换器将5V升压到高于8.2V电压,然后再使用一个限流开关,相对方式1的成本和体积会小很多,但是充电时间可能会比较长,适用于电池容量比较小的场合。

    以上谢谢!

  • TI目前没有单独的BOOST充电IC,推荐先加一级boost,然后用BQ24133去进行锂电池充电管理。