This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61196: 关于200mA持续电流和400mA脉冲电流的问题

Part Number: TPS61196


在使用TPS61196时,我将最大电流(ISET)设置为了400mA,目前点亮LED电流设置为200mA,也就是50%占空比PWM

现在我想要把LED电流调高到400mA,那么PWM占空比就要提高到100%,但是规格书中说400mA只能工作在脉冲模式下

那么我该怎么做才能在安全状态下驱动400mA电流

是调整ISET引脚设置的最大电流值,然后通过调节PWM占空比来得到我需要的电流值吗

           例如:将ISET引脚设置的最大电流设置到500mA,然后调节pwm占空比为80%,实现400mA电流

规格书中并没有关于大电流应用的详细描述,希望有工程师可以帮忙解答一下