This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5146的 FB引脚电源随着输出电流增加而降低,无法输出25A电流

Part Number: LM5146


您好,

最近使用LM5146做一个试验电源项目,48V输入,25A恒流输出,自己做的CC误差放大器,输出通过二极管引入到FB节点。

问题1:现在20A以下都能稳定工作,但是FB引脚的电压是变化的,5A以下FB引脚可以维持在0.8V左右,10A就变成0.7V,20A大概就0.6V,FB引脚不是一直应该维持在0.8V左右吗?

问题2:25A的时候,输出几秒钟瞬间跌落到20A左右,此时CC误差放大器已经失去控制了,量取FB引脚只有0.4V,这个状态是不是进入了占空比限制模式啊?请问一些,这是什么原因,环路设计不合理吗,但是20A以下CC模式都可以稳定工作。



谢谢!!