This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92641的欠压保护UDIM引脚电压是多少?



我输入电压为24V,Vturn-on 电压为20V。

This pin functions as both the PWM dimming input of the LEDs and as
an input UVLO with built-in hysteresis. When the pin voltage rises and exceeds the 1.276-V threshold, 21 μA
(typical) of current is driven out of the UDIM pin into the resistor divider (RUDIM1, RUDIM2) providing programmable
hysteresis

这意思是说当我UDIM电压低于1.276V IC进入保护模式还是其他意思?