Part Number: LM5116
我想用LM5116设计一个48V输入,24V输出,输出电流25A左右。因为电流大,上下管都用多个NMOS并联,如果使用内部7.4V的LDO驱动的话,驱动电流应该不够,但又不能直接接输出(电压大于VCC最大承受电压16V)。请问这种情况我是不是只能增加一个外部电源给到VCCX引脚?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5116
我想用LM5116设计一个48V输入,24V输出,输出电流25A左右。因为电流大,上下管都用多个NMOS并联,如果使用内部7.4V的LDO驱动的话,驱动电流应该不够,但又不能直接接输出(电压大于VCC最大承受电压16V)。请问这种情况我是不是只能增加一个外部电源给到VCCX引脚?