IC的Vin規格有Absolute Maximum Ratings和Recommended Operating Conditions兩種參數值,這兩種參數的區別是什麼?在實際電源應用中要參考哪一種規格來設計?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
IC的Vin規格有Absolute Maximum Ratings和Recommended Operating Conditions兩種參數值,這兩種參數的區別是什麼?在實際電源應用中要參考哪一種規格來設計?
下面是手册中关于二者的说明。
Operation outside the Absolute Maximum Ratings may cause permanent device damage. Absolute Maximum Ratings do not imply functional operation of the device at these or any other conditions beyond those listed under Recommended Operating Conditions. If used outside the Recommended Operating Conditions but within the Absolute Maximum Ratings, the device may not be fully functional, and this may affect device reliability, functionality, performance, and shorten the device lifetime.