Due to design reasons, I do not want to use the overcurrent detection function. How should the ISNS+ and VOUT pins be connected?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Due to design reasons, I do not want to use the overcurrent detection function. How should the ISNS+ and VOUT pins be connected?
Aim to corrupt the differential current-sense voltages, you can please take a look about 7.3.12.2 Inductor DCR Current Sensing
Section 7.3.12.2 does not explain how to connect when not using current detection. I would like to ask whether the ISNS+ and VOUT pins, which do not require current detection, should be connected by shorting them without grounding or whether they should be grounded together.