This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LM5122的设计方案问题

Other Parts Discussed in Thread: LM5122, PMP7921

应用要求:输入12VDC,输出18VDC、60A、2秒。请问可以用什么方案?查阅了一些资料,似乎LM5122可以实现。比如在TI的参考设计库中有这样一个设计:PMP7921 是一种多相位升压转换器。此设计接受 7V 到 8V 的输入电压,并输出 12V,能够提供持续 5 毫秒的 84A 峰值电流。此设计输出 1000W 峰值功率,峰值效率高达 96%”。这个参考设计和我的应用要求很接近了,只是我的应用要求要持续2秒钟。请问在参考设计基础上如何改进可以提高持续时间呢?请各位老师指导,谢谢。