This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25570:关于MPPT的功能理解

Part Number: BQ25570


请我我理解的MPPT功能正确吗,

在 bq25570 中,当 MPPT 设置为 80% 比例时(如将 VOC_SAMP 引脚连接到 VSTOR),其对应的电压范围 0.08V~4.08V(即输入源开路电压 VOC 的 80%,且 VOC 在推荐的 0.1V~5.1V 工作范围内),芯片会在该范围内自动调节输入电压(VIN_DC),以实现功率最大化。