Part Number: LP8866S-Q1
你好,我有下面两个问题想请教
1、我在使用该芯片时用I2C来控制亮度,配置了0X04寄存器中的BRT_MODE=2h = Brightness controlled by DISPLAY_BRT register,然后给寄存器DISPLAY_BRT(0X00)写亮度值,在我写入值超过18000(最大16位65535),寄存器会复位读到都是0XFFFF,背光变暗,写入值小于18000亮度就恢复正常,另外我在使用默认PWM输入模式就没这个问题(而且亮度能达到最大),请问这是什么原因,我使用的是12.5%混合模式,5路LED,AUTO_BOOST_FREQ是400KHZ,AUTO_PWM_FREQ是305HZ。
2、我在使用PWM输入模式来控制亮度时,我的MCU是12位PWM输出,背光芯片有时候不能识别到我1/4095的PWM变化,背光芯片PWM是16位(理论上能识别到变化),判断依据是我从寄存器0X16和0X18(PWM输入和输入Diagnostics)读的值没变化