This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21750-Q1: The chip's output is abnormal.

Part Number: UCC21750-Q1
Other Parts Discussed in Thread: UCC21750

The output of UCC21750 remains low (-4V). Even though I set IN+ = 5V and IN- = 0V, its output still remains -4V instead of 15V. At this point, the APWM pin is floating and unused, with the following parameters: VCC = 4.8V; RST = 4.8V; FLT = 4.8V; RDY = 4.8V; AIN = COM = 0V; VDD = 15.6V; VEE = -4V.