This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

怎么设置才能让BQ25895的输入电流达到3.25A,充电电流达到5A?急急急!



目前我的设置是这样的:

REG00(0X3F) 输入电流限制为3.25A,ILIM PIN引脚功能禁用

REG02(0XFD) 使能ICO算法,使能D+ D-检测

REG04(0X7F)快充电流限制为5056mA