如题,BQ25895本身能否检测到SYS在放电状态?如果可以,通过哪些寄存器读回来
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个料网上规格书不全,是针对特定客户支持。甚至需要签NDA保密协议,因此请联系当地技术支持。
不过你问的问题,你可以检查寄存器有没有相关寄存器读取,如果没有,你只能通过输入电流,和充电电流,两者差值去估算。
如果想再精准一点,可以增加一个电流检测器件,如INA216
BQ25895可以提供充电电流monitor功能,可以结合这个电流来推测system电流情况
你好,我现在可以控制升压,可以读写寄存器,写进寄存器的数据读回来是正确的,但是充电电流就一直为0,没有充电,REG03的CHG_CONFIG已经使能,REG07的EN_TERM也同样使能,但就是没有充电电流,一直没有充电成功,请问我的是出什么问题?