This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

寻高频PWM控制芯片及MOS

Other Parts Discussed in Thread: UCC35705, CSD19534KCS

我正在设计一款高频开关电压,开关频率1.5MHz,输入65Vmax,输出48V/4A,非隔离BUCK。具体电路结构参见附件。

现欲寻找一颗PWM控制芯片(U3),要求:开关频率1.5MHz左右,能够被外同步,能输出峰值1A、平均100mA以上电流,占空比D>95%,电压型控制,最好能有OV、OC能保护、能从65V直接供电等功能。管脚不要太多,以8脚最好。

如果芯片能直接驱动MOS(U4),那就最好!

目前找到一款UCC35705,驱动能力有限,需要外加驱动器,这款片子常用吗?

MOS(U4)现在选用的是Infineon的BSC440N10NS3,发现它比较脆弱。TI是否有相似的管子,以便比较,要求:Rs_on X Qg_tot 尽量小,以便工作在1.5MHz;100V耐压。

非常感谢您的帮助!