This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117: DEMB是什么意思?

Part Number: LM5117

在TI的大多数电源管理驱动IC中,对IC的引脚 介绍都有 DEMB,请问这个DEMB是什么意思,如何应用比较好,能否详细解答一下?

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 关于DEMB引脚,请参考数据手册的解释:

    Optional logic input that enables diode emulation when in the low state. In diode emulation mode, the low-side NMOS is latched off for the remainder of the PWM cycle after detecting reverse current flow (current flow from output to ground through the low- I side NMOS). When DEMB is high, diode emulation is disabled allowing current to flow in either direction through the low-side NMOS. A 50-kΩ pull-down resistor internal to the LM5117 holds DEMB pin low and enables diode emulation if the pin is left floating.