您好,我现在用BQ24195做电源管理,可以正常的充放电,用PMID来做5V输出,当电池电量大于3.5V时,输出正常,但当电池电量低于3.5V时,PMID输出只有3V,VBUS为0,
寄存器值为:
REG00=27;REG01=2B;REG02=60;REG03=11;REG04=B3;REG05=8A;REG06=03;REG07=4B;REG08=C0;REG09=00;REG0A=23
请问是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,关于boost模式下PMID电压跌落的问题已经解决,最后发现是我使用的电压表有问题,造成电压漂移,实际电路是正常的,谢谢您的解答!
另外还有一个问题,在给电池充电时,刚开始充电,BQ24195会进入DPM模式,充电电流有1.4A左右,充电一段时间后才会自动跳出DPM模式,
寄存器设置为:
REG00=27;REG01=2B;REG02=60;REG03=11;REG04=B3;REG05=8A;REG06=03;REG07=4B;
用的是5V/3.1A的适配器充电,请问是什么原因导致充电进入DPM模式的?谢谢!
你好,我想问下,BQ24195可以作为快充芯片吗?
如果输入用5V,给两节18650充电要5个小时。那用9V,充电时间会不会缩短?
谢谢解答!
BQ24195是为5V输入设计的。想要快充,还是得BQ2589X系列。