This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28731-Q1: 空载低功耗应用

Part Number: UCC28731-Q1
Other Parts Discussed in Thread: UCC28730-Q1,

您好!

我需要做一款低空载功耗开关电源,输入电压200V~1200V,输出电压15V,输出电流1A,功率15W。

1、该芯片内部启动开关为700V,是否有更高电压应用的解决方案?

2、在HV引脚外部再串联高压MOSFET是否可实现在高输入电压(1000V~1500V)条件下使用?

3、是否有推荐适合在1000V~1500V高电压条件下使用的低空载应用的电源管理芯片?