12V输入,电流80A,使用2个1m欧姆的MOS管并联作为防反灌MOS。
在60A输出的时候 MOS管的VGS电压为12V,但电流大于67A时,MOS管的VGS电压开始跳动。
难道LM5050-1的驱动输出和输出电流有关系?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
12V输入,电流80A,使用2个1m欧姆的MOS管并联作为防反灌MOS。
在60A输出的时候 MOS管的VGS电压为12V,但电流大于67A时,MOS管的VGS电压开始跳动。
难道LM5050-1的驱动输出和输出电流有关系?
你看这个料的规格书第五页,VGS那一项,VGS和温度是有一定关系的,全温度范围从4-9V不等。我觉得最可能的原因是电流大了,器件温度升高,VGS有一定影响。你看看VGS的波形,只要不是剧烈那种变动的,应该就是我说的问题。
你需要做的是需要找一个Mos,可以满足全温度范围下能够用VGS(如4-9V)的完全驱动的器件。