This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409多路一起使用时有电流下降的问题

Other Parts Discussed in Thread: LM3409, LM3431

使用4片lm3409驱动4路LED电流分别为1.4A、0.6A、1.4A、1.0A,当两路1.4A同时驱动LED时,其中一路驱动电流会下降50~100mA,单独驱动是电流不下降,请教各位大侠帮忙分析一下,是什么原因。其中U3和U4为两个驱动电流为1.4A和1.0A,当这两路驱动的LED同时亮的时候,就会有电流下降的问题,单独驱动没有电流下降的问题。

  • 楼上的是我同事,描述有不准确的地方,我更正一下。

    U1、U2两个驱动电流都是1.4A,一个是19.2V,一个是12.8V;U3是0.6A、U4是1A。

    其他3路都还好,只有U2单独工作和与其他3路一起工作时电流会下降50~100mA。

    也翻过论坛的旧贴,跟下面帖子现象相似:

    http://www.deyisupport.com/question_answer/analog/led_lighting/f/76/t/22418.aspx

    是否也存在共模干扰。

    为彻底解决问题,是不是可以采用LM3431等单电源驱动多路的方案。但是我看了LM3431的参数,电流好像没有这么大,有没有更合适的芯片?前提是单电源驱动多路,每路独立PWM输入,电流大于1.5A,电压大于20V。

  • Hi

         前端的供电是否有功率的限制(担心电流不够)?

         另外将输入电容Cin增加到10uF以上看一下效果?