Other Parts Discussed in Thread: EV2400
你好,
在设计中把隔离芯片ISO1541D(U9)的Pin6和Pin7断开,正常供电时,芯片BQ7693003(U10)SDA和SCL都有相应波形出来,但是BQ769X0 Evaluation Software收不到数据。请问是什么原因导致的呢?
原理图如下:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
芯片BQ7693003(U10)SDA和SCL都有相应波形出来
可以认为EV2300或EV2400工作了,那么BQ7693003是否有ACK?
请检查I2C地址是否正确。
您好,
ISO1541D是双向I2C隔离器,6 7 脚的状态也会影响2 3脚的状态。
所以,6 7 脚是高电平吗?
SDA脚电平为常高0.8V
对于3.3V供电来说,这个电平不是高电平,