This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24196: BQ24196 寄存器08误报充电充满

Part Number: BQ24196


你好,我在使用BQ24196电源管理芯片管理充电的时候,当我在读取寄存器08的值时,寄存器08的第四第五位为11,按照datasheet的描述当前的充电状态为Charge Termination Done,我可以理解为电池充满电了吗,还是说存在其他的充电终止的条件停止充电。这个时候在正常的情况下,电池都达到了充满电的电压。但是经常也会有异常情况:电池电压还没达到充满的状态,且充电的电流还是保持在涓流充电状态或者是快充状态,还在继续充电。并且寄存器08的第四第五位的值经常会在“11”与“10”跳动( Charge Termination Done 与 Fast Charging状态不停跳动)。我该怎么才能解决这种异常情况呢,使得充电可以稳定且正常进行,不会发生误报?