This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM5010
我的板子要求是20V到60V输入,输出5V.用横流负载放电,300ma电流工作正常,大于300ma输出电压就降到0V了
电流从0到300ma的过程中,电压一直是5V吗,有没有出现4.9V,4.8V等下降的现象
几乎没有下降,就是电流大了一下子直接变为0V,我之前一直是用40V电压输入在测,我今天把电压调到15V就可以输出5V1A了,这个不是能到75V吗,为什么电压才40V就不行了呢
把Ron减小一半试一下
刚刚把RON减小了一半还是一样,输入电压小于19V没问题,输入大于19V时输出输出电压开始下降,到20V时输出电压就差不多没了。
到20V时,测量一下Ron引脚的电平值,电压变大之后,输出跌落,可能和PCB布局布线也有一些关系
15V到19V时电压是1.76,到20V时电压变成了1.84V。这个会和线路板的布局有关系吗
检查输入端的电容C1和C5,核实是否焊接了耐压值为100V的电容,如果焊接了耐压值只有20V或25V的电容,可能出现电容击穿的情况
这个电容是没问题的,都是耐压100V的。下图是电感的输入波形,每格20V,输入电压是18V输出电流1a.这个波形毛刺太高了吧。
毛刺很大,和PCB布局布线有很直接的关系
想请教一下,我的故障会是这种毛刺造成的吗。下面是布局图,帮忙指点一下!我现在主要遇到的问题是输入电压小于18V的时候可输出5V1A,输入大于18V的时候,输出会电压快速下降,用0.1A电流放电的时候输入电压调到40V都没事。
http://www.ti.com.cn/cn/lit/ug/snva101a/snva101a.pdf
PCB布局可以参考EVM板,电感的中间下方尽量不要走线,反馈电阻R1和R2和LM5010尽量接近,自举电容C6尽量靠近5010并避免走过孔
建议将此片LM5010取下来焊接到可以正常工作的板子上,看看工作是否正常,以判断是否为IC的问题,还是板子的问题