This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25172:镍氢电池充电问题

Part Number: BQ25172

镍氢电池3串2并,1300mA/h 问题1:电池电压充到4V后,重新充电,就不能充电,如果一直充就可以充满,

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • BQ25172的配置: 1.)ISET - 375k,这是一个非常低的800uA的充电电流。这是正确的值吗? 2.)VSET - 18k,这是3节电池+间歇充电,看起来还好 3.)TMR - 36k,这是4小时定时器设置。对于1300mAh的电池来说这个看起来很短? 刘阳说道: 电池电压达到4V后,不能再充电。然而,如果让它持续充电,它可以充满电, 如果电池电压高于1.33V /电池,BQ25172将不会开始充电,对于3电池配置,该电压约为4V。 你能告诉我更多关于“继续充电”的情况吗?