我需要正负10伏的电压,很稳定,纹波小,最好是ldo。有这样的ic吗?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi‘
可以采用TPS54160系列,设计见文档: http://www.ti.com.cn/cn/lit/an/slva369a/slva369a.pdf
具体是TPS54060/1 ,TPS54160等等哪一款,视你的电流需求而定。
如果对noise要求很高,在增加LDO, 如上面的电路,加一级LDO,刚好到10V. (设计到10.5V LDO左右功耗最小)
或者在DC/DC的输出不用LDO, 增加以及LC滤波也可以.
你好,
如果电流非常小,用两颗LDO来实现也行,24V转10v用一个,34v转10v用一个,不过电流一般也就能抗10ma左右,所以需要知道你的电流需求多大,谢谢。