TPS65400有四路输出,器件资料上说一、二路可输出4A,三、四路可输出2A。我实际应用时,供电9V,一路输出3.3V,二路输出5V,三路输出2.5V,四路输出1.2V。3.3V和5V均不能输出大电流(实验用500mA已不能正常输出),2.5V和1.2V不能输出1A以上大电流。将三、四路也改为5V输出,也不能输出大电流(实验用500mA已不能正常输出)。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
PowerPad 接GND的散热设计也要注意。
你好,
不能正常输出是什么现象,有可能是thermal pad的焊接问题,也有可能是电感选择的问题,设计是否合理?