This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982调试问题!

Other Parts Discussed in Thread: TPS65982

      最近调试TPS65982一直没有成功,一直只有5V输入输出,不知道是软件配置问题还是硬件问题,希望大神们帮我看下。具体描述如下:

单板设计是DRP模式,单板上电都正常,单板对单板只有5V输出,单板对TI参考板也只有5V输出,TI参考板对单板就不正常了,一直重启一样5V时有时无不稳定,附上原理图、框图和配置文件,希望大家帮忙看下,先谢谢啦!     由于格式的问题我把后缀改了,4276.1.h改为1.json,7635.2.h改为2.ctb

  • 我来顶一下,国内没有人在用这个芯片吗?怎么没人回复呢?

  • Hi Chaolin,

    你自己的板是设置在DRP模式,其中的SINK cap和SRC cap分别是怎么设置的?

    如果是配合TPS65982的EVM板,需要遵循以下表格,将TPS65982设置成DFP模式, source能力支持5V/12V/20V,然后在你的板上sink能力设置成同样的能力,即可观察到高压输出了.注意TPS65982EVM板需要接20V直流电源,J6跳帽要连接上.

    另外你上传的Ctb和jon文件是基于哪个firmware 生成版本生成的?